FBUS.AOUT#.VALUE

Description

This command allows reading the analog output value the fieldbus is setting. This is used as the actual analog output value if AOUT#.SOURCE is set to 2 (Fieldbus).


  • Writing to this command is possible but is not the intended use. When not using the fieldbus, set the analog output value by using AOUT#.SOURCE 0 (User) and set AOUT#.VALUEU to the desired analog output value.

Versions

Action Version Notes
Implemented 02-04-06-000

 

General Information

Type

Read/Write

Units

V

Range

0 to 10V

Default Value

5V

Data Type

Float

Stored in Non-Volatile Memory

No

Variants Supported

Fieldbus variants: AKD2G-SPP, AKD2G-SPE, AKD2G-SPC

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

FBUS.AOUT1.VALUE

3800h

02h

Signed16

-

1000:1

Read/Write

Yes

FBUS.AOUT2.VALUE

3801h

02h

Signed16

-

1000:1

Read/Write

Yes

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

FBUS.AOUT1.VALUE

24150

5E56

Signed16

Read/Write

-

FBUS.AOUT2.VALUE

24151

5E57

Signed16

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

FBUS.AOUT1.VALUE

24150

Float

Read/Write

-

FBUS.AOUT2.VALUE

24151

Float

Read/Write

-